Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80582members
346478posts

MQTT Configuration with Azure for EMSE (Vijeo XL)

budimanc
Ensign
Ensign
0 Likes
6
1650

MQTT Configuration with Azure for EMSE (Vijeo XL)

Dear Schneider,

 

I need some help in MQTT driver configuration for Ecostruxure Machine SCADA Expert.

 

Hereby i attached some photos from my Azure portal and also the configuration that i insert from Azure to EMSE.

I still not able to received data from Azure in my EMSE tags.

Hope someone in this forum will help to guide me.

 

Thx.

 

Best Regards,

 

Budiman Chandra

Tags (2)
6 Replies 6
Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
0
1632

Re: MQTT Configuration with Azure for EMSE (Vijeo XL)

Hi @TomDroll Could you support on this?

Thnaks!!!!!

Rodrigo G. 


Industrial Automation Community manager

Tags (1)
TomDroll
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
4
1625

Re: MQTT Configuration with Azure for EMSE (Vijeo XL)

Hi Budiman, I am not sure if the pictures didn't get posted or if I just cant find them.

 

A couple of questions, is it safe to assume that the MQTT Broker is running on Azure?  Have you been tried using a free MQTT client like MQTT.fx or MQTT Explorer on the same PC as the EMSE Runtime to confirm you connection to the broker?

 

Testing with a client like mentioned above will help determine if the issue is the connection to the broker or the configuration in EMSE.

 

What version of EMSE are you using? 

 

 

I will look for your reply.

 

TD

Tom Droll
Tags (1)
budimanc
Ensign
Ensign
0 Likes
3
1616

Re: MQTT Configuration with Azure for EMSE (Vijeo XL)

Dear @TomDroll 

 

Hi, thx for the reply n guide for testing using free MQTT client.

It will takes sometime to use free MQTT client to EMSE.

 

I'm using EMSE v8.1 with Service Pack 2.

Hereby i attached the configuration I've made by using MQTT Azure to EMSE.

 

Waiting for your reply soon.

 

Attachments
Tags (1)
budimanc
Ensign
Ensign
0 Likes
2
1584

Re: MQTT Configuration with Azure for EMSE (Vijeo XL)

Hi @TomDroll 

 

Still waiting for your guidance.

Thx.

TomDroll
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
1
1529

Re: MQTT Configuration with Azure for EMSE (Vijeo XL)

Hi Budimanc, sorry for the delay in response (was on holiday).  I did some research on this topic and it seems that the MQTT library that Azure IoT Hub is different than the EcoStruxure Machine SCADA Expert driver implementation.  We are currently working to resolve the issues and will follow up when an update is released.

 

Sorry for the troubles.

 

Is this an active project or testing for a future project?

 

Regards,

Tom 

Tom Droll
Tags (3)
budimanc
Ensign
Ensign
0 Likes
0
1466

Re: MQTT Configuration with Azure for EMSE (Vijeo XL)

Hi @TomDroll 

 

I have change my MQTT connection by using AWS IoT Core.

I have also tried to connect AWS Iot Core to publish/subscribe by using MQTT Box and succeed.

But i am still failed in connecting Vijeo XL to AWS Iot Core.

Where should i upload certiicate for VIjeo XL, since AWS Iot Core is using Self Signed Certificate method.

 

Hereby i try to add new certificate in the Vijeo XL, but seems like the port change to 443 (it should be 8883).

Thx.

 

Best Regards,

 

Budiman Chandra

Attachments
Tags (1)