Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-02-25 05:05 AM
Hello,
I'd like to connect a HMIST6400 (programmed with ESOTE) with a TM221CE24R PLC (programmed with MachineExpert Basic).
I have exported the PLC symbols, but MEB allows only the .csv format which is not recognized by HMI.
How could I connect these two devices?
Posted: 2021-02-26 04:28 AM . Last Modified: 2021-02-26 04:33 AM
The way is easier than you expect.
Add a SE Modbus TCP driver (or SIO)
And then import the Basic file via symbol import
Posted: 2021-02-26 04:28 AM . Last Modified: 2021-02-26 04:33 AM
The way is easier than you expect.
Add a SE Modbus TCP driver (or SIO)
And then import the Basic file via symbol import
Posted: 2021-02-26 04:51 AM
Dear @jhonut ,
I have made the next video of how to connect the HMISTO7 to a M221.... is the same for the HMIST6****:
https://schneider-electric.box.com/s/av7nek0zbdltp6oh7qfuysfiimx2uomh
Best regards,
Letomas
Posted: 2021-02-26 04:53 AM . Last Modified: 2021-02-26 05:04 AM
Thanks for your reply, @Bastian_Schmitz !
I have done as you suggested but I get an error: "Invalid device address. Enable or disable IEC address mode in the equipment." How should I do this? It's true that I don't use Modbus addresses but memory addresses.
Later edit. I have seen the video suggested by @LeTomas and I've how he's done it.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.