Hi,
I'm currently trying to set-up a M241 PLC to communicate with a Rigol Multimeter via RS-232 using the ASCII manager.
I have had success sending commands to the multimeter (and hyperterminal on a PC) from the PLC using the example below from the
SoMachine Modbus and ASCII Read/Write Functions PLCCommunication Library Guide
I have taken this example and modified it in order to try and receive a basic message, initially from hyperterminal, See 'Current receive example' below, however I am yet to get this working.
Can anyone share an example of code used to receive a message using this SEND_RECV_MSG function block? Or provide a hint as to where I am going wrong?
Send Example:
Current Receive Example:
The PLC is connected to my computer using a RJ45 to serial cable and a serial to usb converter.
I believe I have the ascii manager and cable set-up correctly as I am able to send messages from the PLC to hyperterminal.
Thanks in advance,
Kiwi_Karl
Hello,
You can use programme that at linked.And also You can find video at attached for explaining programme.But video is turkish language.
Best Regards,
Hi ismailozinan,
Thank you for the program. It was very helpful, I've got it working now!
Regards
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!