41348members
184425posts

EcoStruxure Machine Expert WebVisu project example used on STW6.

Cadet

EcoStruxure Machine Expert WebVisu project example used on STW6.

Is there any EcoStruxure Machine Expert WebVisu project example used on STW6 HMI?

Or maybe some example manual for use of visualisation in EcoStruxure Machine Expert?

1 REPLY 1
Highlighted
Cadet

Re: EcoStruxure Machine Expert WebVisu project example used on STW6.

Hi Boban988,

 

Here is a guided video on that very subject:

https://www.youtube.com/watch?v=eRzwDBD8JBQ

 

Note that the video shows SoMachine v4.3. In EcoStruxure Machine Expert v1.1, the WebVisualization feature can be applied in the same way.

 

And here is another video that goes into more depth on the WebVisu feature of SoMachine/EcoStruxure Operator Terminal Expert:

https://www.youtube.com/watch?v=sxvk7_aTFpo