Hi,
I'm having an issue with the FBD Editor in Control Expert V14.1.
Note: My colleagues have the same issue.
The FBD Editor is not allowing me to click and select the input/output pins of a FB.
Instead when the left mouse button is pressed, the cursor changes to that shown when the "Link" tool is selected.
Below a screenshot of the cursor when the left mouse button is clicked.
.
In previous versions of Unity Pro a single left mouse button click on a FB input/output pin selects the pin.
Has anyone else had similar issues?
Does anyone know of solutions to this issue?
Solved! Go to Solution.
Speaking to Schneider Tech Support, they advised that to select a FB pin you must click on the pin description inside of the FB square.
Clicking on the FB pin itself will begin creating a link to another FB.
This is a new 'feature' that first appeared in V13.0.
Speaking to Schneider Tech Support, they advised that to select a FB pin you must click on the pin description inside of the FB square.
Clicking on the FB pin itself will begin creating a link to another FB.
This is a new 'feature' that first appeared in V13.0.
So basically:
Hope this helps.
Richard
Oops ... and one more I forgot is that you can right-click either to get the options menu.
Richard
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!