43453members
218021posts

Control Expert V14.1 DDT Data Editor

Highlighted
Ensign

Control Expert V14.1 DDT Data Editor

Hi,

 

Has anyone experience the following and know how to prevent it from occurring?

 

When re-ordering elements within a DDT Structure in the DDT Data Editor the comment of the element that is moved disappears. 

5 REPLIES 5
Highlighted
Crewman

Re: Control Expert V14.1 DDT Data Editor

Hi @bprobertson ,

 

My DDT editor does not behave the same as your's at all - when dragging elements of the DDT around, Control Expert actually makes copies of the elements. It does not reorder the elements.

However, those copies do not contain the comments of the element original elements.

 

See my video attached 

Highlighted
Ensign

Re: Control Expert V14.1 DDT Data Editor

Hi @MarkPitout,

 

Clicking and dragging items will duplicate items. 

Pressing shift before releasing the mouse button will instead move items.

Highlighted
Crewman

Re: Control Expert V14.1 DDT Data Editor

Okay. Did the shift-release thing - my Unity behaves the same as yours (comments are removed from the variable once moved).

 

I'll see if I can raise a ticket for this - given that this behavior isn't critical to how a PLC runs the code, I don't expect it will be high on the developers list of priorities. But let me raise it none the less. perhaps it will be sorted in a future hotfix or release

Ensign

Re: Control Expert V14.1 DDT Data Editor

Hi @MarkPitout,

 

Correct it doesn't affect the behaviour of the PLC code however, from a development point of view it reduces productivity as you need to re-add comments if a change is made.

Highlighted
Ensign

Re: Control Expert V14.1 DDT Data Editor

Hi @MarkPitout,

 

Did you end up getting a response from the ticket that you raised regarding this?

Tags (1)