42321members
209667posts

Control Expert FBD for PM5320?

Crewman

Control Expert FBD for PM5320?

Hi,

Does it exist a function block for power meters PM5320?

Have you any example and documentation?

The application is with a M580 PLC.

Best regard,

Samuel

1 REPLY 1
Highlighted
Ensign

Re: Control Expert FBD for PM5320?

Look at the Modicon GPL libraries - Device library.

There are two DFB's available, one for ModBus serial communication and one for Ethernet communication.

The libraries are available via Exchange (Free)

https://shop.exchange.se.com/en-US/apps/44667/general-purpose-library-for-ecostruxure-control-expert