43369members
217837posts

Control Expert FBD for PM5320?

1 REPLY 1
Highlighted
Ensign

Re: Control Expert FBD for PM5320?

Look at the Modicon GPL libraries - Device library.

There are two DFB's available, one for ModBus serial communication and one for Ethernet communication.

The libraries are available via Exchange (Free)

https://shop.exchange.se.com/en-US/apps/44667/general-purpose-library-for-ecostruxure-control-expert