43545members
218143posts

The importance of Loop Indicators

Lieutenant
Lieutenant

The importance of Loop Indicators

Originally published on GMI blog by GM International | July 23, 2020

 

Limpotanza-degli-indictori-di-processo.jpg

 

Loop or Field Indicators are essential to control and monitor normalized or field signals to provide immediate data in both hazardous and safe area.

Such indicators measure, analyze and calculate analogical signals. They can also loop power two-wires sensors.

Their Input channels allow the measuring of current, voltage, RTD (Resistance Temperature Detectors), TC (ThermoCouples) and provide also for alarms and digital interfaces. Limit values can be monitored to trigger relays or OC transistors. Analog outputs can also transmit process signals.

 

Indicators have different characteristics and specifications. The majority of them are in-field configurable but some versions can be programmed through PC. Most of the times indicators are loop powered devices that process 4-20 mA signals. Enclosures can be of different materials (polycarbonate, aluminum or stainless steel) to allow for installation in the harshest conditions. LED or LCD displays make it easy to monitor different signals thanks to analog and digital outputs. Using proper measure converters, indicators can transform the measures from the field in standard signals. Remote monitoring and configuration are possible thanks to various technologies such as ModBUS, HART and Foundation Fieldbus.

 

 

The correct installation 

Typically, digital indicators are designed to be non-incendive (Ex-nA) meaning that they cannot represent an ignition source while active in precise circumstances.

In typical installations, digital loop indicators are integrated as passive elements, with or without external power, directly in the 4-20 mA current loop.