EBO Idea Exchange
Have ideas on how to improve the EcoStruxure Building Operation? Please share and get votes from our Community to influence development efforts.
Visit the brand new Software & Firmware Center, within EcoXpert Extranet
What are the main changes vs the previous solution :
For a better user experience and usability, files will be organized by “Software packages” related to versions (ex : EBO 2022).
A package now includes all needed items for the installation of a given version:
User | Likes Count |
---|---|
6 | |
5 | |
4 | |
2 | |
2 |
I think it would be great if you could somehow dynamically include external sections of TGML code into a graphic page. I imagine it working somewhat like a #include statement in the header of a C program.
Use case would be a complex menu structure that could be included into the top of every other graphic in the system. I know that the panels are meant to address this sort of use case, but there are limitations there with being able to create very complex menus that include drop down sections. These often fall behind the outer limits of the panel, but if it were native to the rendered page, it would work great, and be very easy and quick to update many pages. Could also be something like a weather component that may need to be updated in the future and would provide a way to update every graphic at once.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.