EBO Idea Exchange
Have ideas on how to improve the EcoStruxure Building Operation? Please share and get votes from our Community to influence development efforts.
Visit the brand new Software & Firmware Center, within EcoXpert Extranet
What are the main changes vs the previous solution :
For a better user experience and usability, files will be organized by “Software packages” related to versions (ex : EBO 2022).
A package now includes all needed items for the installation of a given version:
User | Likes Count |
---|---|
6 | |
5 | |
4 | |
2 | |
2 |
Hi
I have (at many sites) seen, that the values in the graphic, trendlogs, I/O module ect. is not stable. It "jumps" up and down.
We have a lot of costumers, that asks/complains about this and it looks like our measurements are unstable.
We are using AS-P + I/O modules, but it might be the same for AS-B.
I think this should be changed, so we don't have these problems any more.
I can think of three possible solutions:
1: Add a TimeConst (adjustable) directly on the inputs of the I/O module.
2: Change the binding from the "FunctionBlokProgram", so it refers to the OUTPUT of the block instead of the INPUT of the block (See attached printscreen "SBO FBP - RI binding.png").
3: Make the measured value from the I/O module more stable by adding more samples. (I think this solution would help a lot, but is cannot replace solution 1 and 2!)
Solution 2 have been made as a defect 31966. The answer from PSS is that it will not be changed
Solution 3 have been made as a defect 31940. R&D is still investigating this issue.
If anyone can relate to the problem, please "vote" for this idea
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.