EBO Idea Exchange
Have ideas on how to improve the EcoStruxure Building Operation? Please share and get votes from our Community to influence development efforts.
Visit the brand new Software & Firmware Center, within EcoXpert Extranet
What are the main changes vs the previous solution :
For a better user experience and usability, files will be organized by “Software packages” related to versions (ex : EBO 2022).
A package now includes all needed items for the installation of a given version:
User | Likes Count |
---|---|
6 | |
5 | |
4 | |
2 | |
2 |
How it works
A single LON add-on module for MP-X and RP-X and the AS-B(L).
• Develop one LON module for Xenta and MN LON refurbish as well as LON integration to EcoStruxure for Buildings Operation on the field device level
• New product to enable ongoing manufacture as long as EBO is supported
• No need to develop other LON devices (spare devices for Xenta 280/300/400 and MN LON refurbish)
For more details please see the attached file.
update 31.07.2018:
MP-C:
Search - Asset Library | EcoBuilding - The Exchange
MP-V:
Search - Asset Library | EcoBuilding - The Exchange
update 21.12.2017:
To get an impression of the capabilities from the MP-X controller range you can watch this video DONE: 2017.10.12 KRS - High Level Overview for Upgrading SmartStruxure Sites
beginning at ~41 minutes showing the MP-X posted by Allison Sartor
old Post (created 09/10/2017):
A single LON add-on module for the AS-B(L), and future room and zone controllers.
• develop one LON module for Xenta refurbish and LON integration to EcoStruxure for Buildings on the field device level
• New product to enable ongoing manufacture as long as ESB is supported
• No need to develop other LON devices (spare devices for Xenta 280/300/400 refurbish)
Originally posted 2017-10-10 10:46:00.000 UTC
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.