EBO Idea Exchange
Have ideas on how to improve the EcoStruxure Building Operation? Please share and get votes from our Community to influence development efforts.
Visit the brand new Software & Firmware Center, within EcoXpert Extranet
What are the main changes vs the previous solution :
For a better user experience and usability, files will be organized by “Software packages” related to versions (ex : EBO 2022).
A package now includes all needed items for the installation of a given version:
User | Likes Count |
---|---|
6 | |
5 | |
4 | |
2 | |
2 |
If Schneider Electric claims to support HTML5 based graphics, then it should ACTUALLY be supporting HTML5. It is not possible to simple things like <input></input> (input fields). This is one example that the claim is not true. Along with that, modern browser supported technologies should be supported as well. This includes, but not limited to:
-JavaScript 6 (not the JavaScript 1.5 from 2000 that no one has used in over a decade)
-Importing of addition, external libraries and frameworks like AngularJS, React, Twitter Bootstrap, etc...
-Any and all HTML5 features and tags
-CSS3
-Java
-Python
-Any other languages that can work with HTML5
-Encryption
Essentially, the TGML idea is far past not holding up to the claim the it supports HTML5. This should be seriously looked into because graphics creation is extremely limited in its current TGML form.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.