EBO Idea Exchange
Have ideas on how to improve the EcoStruxure Building Operation? Please share and get votes from our Community to influence development efforts.
Visit the brand new Software & Firmware Center, within EcoXpert Extranet
What are the main changes vs the previous solution :
For a better user experience and usability, files will be organized by “Software packages” related to versions (ex : EBO 2022).
A package now includes all needed items for the installation of a given version:
User | Likes Count |
---|---|
6 | |
5 | |
4 | |
2 | |
2 |
I don't know if it could be helpful others or not but I would use it if I can.
My problem is that if I have a data point (e.g. an input) and I want to use it in my application (FBD or script) then I have to create the point under the I/O module, create it in the application and bind them together.
It could be easier to create the point (phisical or logical) and after that drag and drop it to the application. Workstation has to create the datapoint in the application with the same name and bind it to my datapoint.
With this I don't have to create the point twice and bind them.
Multiple selection could make it more useful.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.