EBO Idea Exchange
Have ideas on how to improve the EcoStruxure Building Operation? Please share and get votes from our Community to influence development efforts.
Visit the brand new Software & Firmware Center, within EcoXpert Extranet
What are the main changes vs the previous solution :
For a better user experience and usability, files will be organized by “Software packages” related to versions (ex : EBO 2022).
A package now includes all needed items for the installation of a given version:
User | Likes Count |
---|---|
6 | |
5 | |
4 | |
2 | |
2 |
APC, part of Schneider, lines of products: PDU, UPS, environmental monitors communicate over SNMP.
I have costumers who want to be able to control them through the Automation Server, example the AS reads from the UPS that the UPS battery is low or that the temperature in a room is to high and starts turning off outputs on a power outlet and then over modbus it may also open G3 circuit breakers.
The idea would be add an SNMP interface just like there is a Modbus and BACnet one already. Using as a reference the Modbus Interface, you would add a client then set in its properties the host and auth settings, Then under the device have the options to add points of the different types and instead of putting a register address inputting the OID.
The main goal is better integration of Schneider different lines of products and for the AS to tap into the wide range of SNMP devices.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.