EBO Idea Exchange
Have ideas on how to improve the EcoStruxure Building Operation? Please share and get votes from our Community to influence development efforts.
Visit the brand new Software & Firmware Center, within EcoXpert Extranet
What are the main changes vs the previous solution :
For a better user experience and usability, files will be organized by “Software packages” related to versions (ex : EBO 2022).
A package now includes all needed items for the installation of a given version:
User | Likes Count |
---|---|
6 | |
5 | |
4 | |
2 | |
2 |
A nice feature of the default Alarm View is that it can pop up in a floating window anytime a new alarm is generated. This is great feature for a critical site with 24/7 monitoring.
The problem is when everyone else is logged into the system the window keeps popping up, taking the full focus of the computer and makes it almost impossible to get any work done.
I would like to have this setting available for all user generated alarm views not just the default alarm view. This way we can enable it on an alarm view for the the operators that monitor the system 24/7 and disable it for the rest of the users that do not track and acknowledge alarms. This way only Workspaces with the "pop-up" alarm view attached to it would see the pop up window.
Right now the setting is greyed out for manually created alarm views.
Standard Alarm View:
Manually Created Alarm View:
Originally posted 2017-02-27 21:24:00.000 UTC
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.