Input voltage displayed is higher than wall outlet
APC UPS for Home and Office Forum
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-06-2903:35 AM. Last Modified:
Friday
Input voltage displayed is higher than wall outlet
- I have a BX1500G UPS that is almost one year old. I am using Power Chute version 2.2
The input voltage on the LCD display shows 122-124 volts (fluctuates) and 268-270 watts. This is not normal for my system. I usually show 120 volts input and 277 watts (during normal operations) consistently. Watts of course increase if I play a game, etc. The output voltage from the UPS shows 122-124 volts as well.
Wall outlet measured with a multimeter shows exactly 120.0 volts AC.
Why has this changed? I did have to reinstall Power Chute 2.2 yesterday (after Windows 7 reinstallation). After the reinstall, the display read the usual numbers, if I remember correctly. A self-test right after having installed Power Chute was successfull.
Below is the current status from Power Chute:
Model: Back-UPS BX1500G
Serial number: 3B########
Firmware revision: 866.L1.D
Software version: PowerChute Personal Edition 2.2
Date of last manual self-test: 6/11/2010
Result of last manual self-test: Passed
RAM: 8 GB
Free disk space: 1,687,122 MB
- and -
Electrical power is being supplied by: AC Utility Power
Remaining battery charge is: 100 %
Battery is currently: Charged
Last transfer to battery was caused by: None Recorded
Result of last manual self-test is: Passed on 6/11/2010
Input Voltage: 123 volts