Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-06-2807:37 PM. Last Modified:
Tuesday
Comment: Back-UPS ES BE750BB 450W/750VA
I generally handle Smart-UPS series, but was helping a friend with finding a UPS for his home PC, so I had a chance to look at a few different ones from a few different brands. I'm quite impressed with the Back-UPS ES 750VA BE750BB's specs. On this model, APC got away from the annoying new trend of mating a tiny battery with higher VA ratings offering quite a respectable runtime.
This is what he wanted to get:
TrippLite Smart1000LCD 500W/(1000VA) MSRP $184. Not bad. Until I looked at the specs
They used a VA to W ratio of 2, which is unrealistically high. VA rating makes for bigger value on the package, but watt is what matters when it comes to runtime.
Having runtime far in excess of the frequent <1min outage with lower level of discharge means the battery lasts longer.
Full : 6 min (450 Watts)
Half: 19 min (225 Watts) , 12 min (300 Watts, something between 12-19min at 250W)
Since he was working around $200 budget and wanted the voltage regulation, he got the APC Back-UPS BR1300LCD(13 minutes @ 500W), which gets better runtime than the TrippLite SmartPro Smart1500LCD that costs more and runs 13 minutes @ 450W.