APC UPS for Home and Office Forum
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 05:53 AM . Last Modified: 2024-03-21 10:49 PM
I have the BX1500G and am running Windows 7 x64 SP1 with Powerchute Personal 3.0 (PP3). I just tested what happens when power goes out while the computer is in sleep mode, and this is what I found:
1. I manually sleep the computer.
2. I manually trip the breaker to the room. (Getting to the wall outlet would require me to pull my desk out, which isn't easy.)
3. The computer has resumed from sleep in the 10 sec or so it takes me to get back to the room.
4. The computer hibernates after 2 minutes per configuration in PP3.
5. I reset the breaker.
6. When I get back, the computer has restarted, despite the BIOS option "Restore on AC Power Loss" being set to "Power Off" and all other wake options being disabled.
7. I use TrueCrypt (TC), so I just wait for a while with the computer at the TC password prompt, which appears right after the BIOS loads, before Windows begins to load. The UPS continues to supply battery power for about a minute.
8. Then the UPS shuts off and turns back on within about a second, transitioning to wall power in the process. This causes the PC to turn off, as well as other connected equipment, such as my cable box, router, cable modem, etc.
9. The PC restarts again, and after I enter the TC password, Windows resumes from hibernation.
This is just horribly wrong, and I confirmed it's real by doing it twice. Items (6), (8), and (9) should not be happening, and I can't explain the extended time on battery power after wall power has been restored described in (7). The UPS passes self-test, and the load is around 25%, with remaining runtime of 20 minutes. I guess if I wasn't using TrueCrypt or had entered the password and allowed Windows to boot, the UPS would have turned off and then back on while Windows was loading or I was using Windows, defeating the purpose of the UPS. It makes no sense at all.
I also tried it with the PC off, and with it on but sitting at the TC prompt. None of this nonsense happened. Of course, the UPS didn't power the PC down, but it resumed wall power instantly, without the UPS turning off and then back on.
Is this a known problem? What to do?
Message was edited by: timj
Message was edited by: timj
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 05:53 AM . Last Modified: 2024-03-21 10:49 PM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 05:53 AM . Last Modified: 2024-03-21 10:49 PM
To test whether the BIOS "Restore on AC Power Loss" setting is working correctly, I booted to the TC password prompt, and then I unplugged the PC from the UPS. I waited 30 sec and plugged the PC back in, and it did not restart. I also booted into Windows and manually hibernated the system. After it shut down, I unplugged the PC from the UPS, waited 30 sec, and plugged it back in. The PC did not restart then, either. So that's working right.
I can only conclude that in the Windows scenario described in my first message, PP3 is somehow programming the UPS to send a USB signal to restart the PC when power is restored, which is just completely unwanted and improper. I don't see any other explanation for why the PC is restarting.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 05:53 AM . Last Modified: 2024-03-21 10:49 PM
this might have to do with the shutdown timeline for these units:
Shutdown time line, software not installed:*
1. UPS goes to battery, the on battery beep sounds
2. The UPS will sound the on battery beep until it reaches the last few minutes of run time. The length of time depends on the load and how old the battery is.
3. When the unit reaches the last few minutes of battery life it will then sound its low battery alarm.
4. Just before the battery is completely exhausted the ups will turn itself off.
5. If the UPS went to battery due to a brown out the unit at this point will be in LVSM until the voltage becomes acceptable again.
PowerChute Personal Edition default shutdown time line:*
1. UPS goes to battery and PCPE starts its preserve battery power counter.
2. When the counter expires it sends a command to the UPS to start counting its turn off delay and then commands the OS to shutdown.
+3. The operating system shuts down and the UPS continues to count its turn off delay. (Once the UPS finishes counting its turn off delay it will reboot and nothing can stop this from happening.)+
4. The UPS cuts power to the outlets then rechecks to see if the incoming power is acceptable. If it is not it waits there until power returns.
5. If the UPS went to battery due to a brown out the unit at this point will be in low voltage sleep mode until the voltage becomes acceptable again.
i read the post quickly but this is what it sounded like to begin with.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 05:53 AM . Last Modified: 2024-03-21 10:49 PM
It sounds like the problem here is that the computer restarted itself from hibernation before the UPS turned itself off and back on. That's odd--I'm curious why. Does it happen exactly when power is restored to the UPS? The up-side is that Truecrypt is nicely suppressing Windows from loading so at least there should be no adverse consequences.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 05:53 AM . Last Modified: 2024-03-21 10:49 PM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 05:53 AM . Last Modified: 2024-03-21 10:49 PM
Hi timj, a simple test we can try to see how the computer and UPS are interacting is to manually put the computer into hibernate mode. Once in hibernate mode, with the ups still online and on AC power, unplug the computer and replug it back into the UPS. From here we should be able tell if it is the BIOS giving up issues (as once the computer is in hibernate mode, the ups has no way to communicate with the computer). Hope this helps.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 05:53 AM . Last Modified: 2024-03-21 10:49 PM
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.