APC UPS for Home and Office Forum
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 01:38 AM . Last Modified: 2024-03-22 03:13 AM
Hi,
I have a BE650R-CN model APC ups attached to my systems. I came home the other night and everything was turned off that was connected.. ie pc and router. when I tried to reconnect with the wall outlet. (trying to reboot it as it were). The ups emitting a long constant ringing. Not a beeping with intervals. I tested the ups by just plugging into a different wall outlet and a laptop running with the power connected. After being out for a couple of hours I came home and the laptop had powered down and the green light on the UPS was out. Power had drained from the laptop battery. It seems strange that it would drain even if the battery in the ups was bad.
Here is the current status output with nothing plugged into the ups.
DATE : Sat Aug 08 19:35:43 EDT 2009
HOSTNAME : m061839
RELEASE : 3.14.4
VERSION : 3.14.4 (18 May 2008) debian
UPSNAME : m061839
CABLE : USB Cable
MODEL : Back-UPS ES 650
UPSMODE : Stand Alone
STARTTIME: Sat Aug 08 17:41:07 EDT 2009
STATUS : ONLINE
LINEV : 122.0 Volts
LOADPCT : 2.0 Percent Load Capacity
BCHARGE : 100.0 Percent
TIMELEFT : 44.2 Minutes
MBATTCHG : 5 Percent
MINTIMEL : 3 Minutes
MAXTIME : 0 Seconds
SENSE : Medium
LOTRANS : 088.0 Volts
HITRANS : 139.0 Volts
ALARMDEL : Always
BATTV : 13.5 Volts
LASTXFER : No transfers since turnon
NUMXFERS : 0
TONBATT : 0 seconds
CUMONBATT: 0 seconds
XOFFBATT : N/A
STATFLAG : 0x07000008 Status Flag
MANDATE : 2006-01-16
SERIALNO : 3B0603X30613
BATTDATE : 2000-00-00
NOMINV : 120 Volts
NOMBATTV : 12.0 Volts
FIRMWARE : 825.B1.D USB FW:B1
APCMODEL : Back-UPS ES 650
END APC : Sat Aug 08 19:36:12 EDT 2009
I don't want to replace the battery if it's really a problem with the UPS itself. Besides it's almost cheaper to just buy a new ups instead of replacing this battery.
comments would be appreciated
Jeff.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 01:38 AM . Last Modified: 2024-03-22 03:12 AM
This unit performs a Self test at start up and every 14 days automatically. If the unit fails the Self test, it will emit a constant tone with Power on and Replace Battery LEDs flashing alternatively.
Is the UPS powering on fine with normal load attached? or Is the UPS still making a constant beep with load attached after you power on it? Could you please let us know the light indication of the UPS when it is making the constant beep?
If it powers on fine with load attached, then I recommend you to stimulate a Power failure by unplugging it from the wall and check if it runs the equipment on battery as expected.
These information will help us to discover what is going on with the unit.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 01:38 AM . Last Modified: 2024-03-22 03:12 AM
This unit performs a Self test at start up and every 14 days automatically. If the unit fails the Self test, it will emit a constant tone with Power on and Replace Battery LEDs flashing alternatively.
Is the UPS powering on fine with normal load attached? or Is the UPS still making a constant beep with load attached after you power on it? Could you please let us know the light indication of the UPS when it is making the constant beep?
If it powers on fine with load attached, then I recommend you to stimulate a Power failure by unplugging it from the wall and check if it runs the equipment on battery as expected.
These information will help us to discover what is going on with the unit.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.