Visit the Industrial Automation Knowledge Base to get know-hows, hints and tips. It is designed to share vast amounts of technical knowledge and expertise in Industrial Automation products, systems, applications and markets.
With the migration of the GeoSCADA Expert Registry settings away from using the Windows Registry to being an internal Database Registry, there should be some way to change these Registry values from APIs such as the Automation Interface and the .NET API (plus SOAP).
There is currently the internal ViewX scripting GetRegistry and SetRegistry, so I would think that something similar would be desirable from the Automation Interface connection / .NET API connection objects also (where authentication is already associated with this connection object).
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!