The geospatial maps are good, but they could be much better.
One such request would be if the icons could be customised so that they aren't just picked from a list of triangle, square, diamond.. and then a circle..
It should be possible to specify any Unicode character, OR an SVG icon to be provided, and this should be possible to animate (as an index into a map icon table object perhaps) via the map query (i.e. so that if a pump is running we can use a certain icon vs if it's not).
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!