New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] WebX and Database Manager

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: AaronJust, originally posted: 2019-02-25 04:46:57 Id:370
Is it possible to configure IIS to work with ClearSCADA using a database other than (Default)?

I used database manager to create two new databases instead of using the default one, and (kind of as expected) the web services don't work properly (e.g. Schema).


Reply User: geoffpatton, posted: 2019-02-25 16:31:56
The original WebX uses port 80 by default. You can edit it in the Server Configuration. It is under System Configuration and then WebX.


Reply User: JesseChamberlain, posted: 2019-02-26 01:40:08
Schema is on DBServer hosted WebX, so you can change that in ServerConfig as Geoff says.

With IIS hosted WebX you need to mess around with the IIS configuration, which isn't very supported and I wouldn't really recommend. Dustin wrote a [quite good article](https://du5tin.com/2017/06/28/secure-clearscada-webx/ "quite good article") that is relevant.

But really, if you want to do this kind of thing you should upgrade to CS2017R3, where you get a WebX System Configuration tool, which means you don't need to mess around, just add the WebX connection same as you would a client connection.