New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] SDE exports via Automation Interface

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: florian, originally posted: 2018-10-25 20:28:27 Id:306
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

-------------------------------

**_nminchin:_**
**_Hi,_**

**_I have a number of objects that I need to back up and restore to another server individually (~350 or so) and I really don't want to have to do this manually..._**

**_I've looked before at the .NET api / ServerSCX object and the ViewX automation interfaces if this is possible with no luck, but I'm hoping that I've missed something._**

**_Does anyone know if this is possible via one of the automation interfaces? Or via ClearSCADA scripting?_**

**_Cheers_**

-------------

andrewscott:
The .NET Client API has the DBObject.ExportConfiguration method (in the ClearScada.Client.Simple namespace).