New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] Returning the close option to inset windows to the right hand side

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: adamwoodland, originally posted: 2019-03-21 04:48:37 Id:386
This may be a polarising opinions setting, but a new 'hidden' Registry setting that people may want to try. I can't claim I found it myself, just seen it in a email conversation between a colleague and a customer and though I should share.

At the ViewX client...

HKEY_LOCAL_MACHINE\\SOFTWARE\\Wow6432Node\\Schneider Electric\\ClearSCADA\\ViewX\\InsetWindowsHaveChrome

Create as a DWORD, set to 1 and restart ViewX and now any mimics opened as insets get a close on the right hand side. Default is 0.

I do think it looks a little ugly as the current tab is also still shown, and so screen real-estate is also reduced a little. But it may make someone happy when they go to close insets.

Should appear to work in Dec 2018 builds onwards, certainly works in my 2017 R3 Feb 2019 build.


Reply User: sbeadle, posted: 2019-03-21 07:56:38
This feature is in:
2017 R2 November '18
and
2017 R3 January '19


Reply User: geoffpatton, posted: 2019-03-21 14:15:19
There is an argument for Microsoft trained us to close a window from the right since Windows 95. For me I went from DOS to Windows 95, so closing windows has always been on the right. I sometimes catch myself looking for it there when closing an inset.

 

Reply User: adamwoodland, posted: 2019-03-21 21:58:31
Thanks Steve.

What gets me is when moving between Windows and Linux and the options on different sides! So having it on the 'left' in ClearSCADA under Windows really messes with my head.