New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Lt. Commander

[import] Request for possible new field in CLogicFBD

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: ROVSCADAENGINEER, originally posted: 2019-05-30 23:33:42 Id:440
Would it be possible to add a new field as a string containing all the Tag names concatenated for FBD's

this would mean I can check that functionality within the DN consumes all specific points for regions. I can quickly locate any sites that such functionality is missing. Instead of visually inspecting each site.

If there is a query In which I can see this information any guidance would be greatly appreciated.


Reply User: sbeadle, posted: 2019-05-31 07:42:47
You can right-click a Logic program and display references. This will list references from and by the Logic, including those within the program. The Client .Net API also lets you call the same function from a program, so it's possible to write a simple program which lists references to a file.


Reply User: ROVSCADAENGINEER, posted: 2019-06-02 21:27:38
yes that functionality is ok if you want to check individual sites. But for checking several sites at once I was meaning.


Reply User: sbeadle, posted: 2019-06-03 10:58:47
I have placed an example utility to do this in a GitHub repository.
This example could be modified for any similar purpose.

https://github.com/ClearSCADA/utility-examples


Reply User: ROVSCADAENGINEER, posted: 2019-06-05 00:59:12
Thanks for taking the time to do this beadle! very helpful.


Reply User: sbeadle, posted: 2019-06-05 07:32:20
No problem.
Steve! .