New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] Query not showing on Display screen

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: KylePaynter123, originally posted: 2019-01-15 18:14:16 Id:349
Hi guys,

I recently created a screen with some SQL quires showing particular digital points.
It's working fine and showing on the Main but it's not displaying the query on the display.

(The Query is showing blank with a red x in the top left corner of the query.

This seems like a simple fix (Please help)


Reply User: tfranklin, posted: 2019-01-15 19:39:43
Is this an embedded mimic? You can't put a list on an embedded mimic.


Reply User: KylePaynter123, posted: 2019-01-16 12:36:05
No it's a List I created from the graphics menu, with a specific query made for those list.

So in screens when I open (Main it's working, but when I open Display I see the list but it has no information inside ) just a red x


Reply User: KylePaynter123, posted: 2019-01-16 14:28:16
ok progress made !

Apparently I had to Group the folder I created as it was a template.
Once that I did that I could now edit the Main and Display Screens.

I also had to remove the list from the Main as it was showing on the Display.

It's working fine now but the Main has no quires on it (I'm looking into this)


Reply User: BevanWeiss, posted: 2019-01-21 20:21:38
Things will be easier if you have a read through of the built in ClearSCADA help, and 'speak the speak' in regards to what items in ClearSCADA are called...
'group the folder I created as it was a template' is very confusing in ClearSCADA world, there is no such thing as 'a folder', they are Groups (CGroup inheritance), which would technically include Templates and Template Instances.

As noted by others, you can't have query lists on embedded mimics (well you can try, they just won't work). So for a query list to work, it must be on the 'top level' mimic that is being displayed.


Reply User: KylePaynter123, posted: 2019-01-23 17:24:43
Noted Thanks guys

I'm coming along, [at]BevanWeiss thanks for expanding on this