New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] Maps in WebX - CS2017R3

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: philbert, originally posted: 2019-02-28 03:17:18 Id:371
Hi,

I would like to show maps in WebX, they are working fine in ViewX.
I noticed in the help the following : 'NOTE: Mapping and geographic information features are not available in Original WebX.'
Does this mean maps can't be viewed in WebX?
If not is there any plan to enable this anytime soon?

Cheers,
Phil


Reply User: sbeadle, posted: 2019-02-28 09:35:24
Display of maps requires the newer IIS-based WebX. Install this using the separate WebX installer, linked from the DVD/ISO image launcher.