New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] Logic Execution when selected Input Change detection

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: Dmitriy, originally posted: 2018-11-29 14:44:08 Id:328
I have Logic ST in CS2017R2.
Execution Method - On Interval.
"Input Change detection" option selected in properties.
when i add input tag AT%I(IAI.CurrentQuality) IAI it is internal analog point, logic execute every time.


Reply User: Dmitriy, posted: 2018-12-03 08:22:26
i test them in CS 2013r2.3 - Logic execute one time.


Reply User: BevanWeiss, posted: 2019-01-03 22:09:32
So you want it to execute at some interval, but to only run if the CurrentQuality is different from the previous CurrentQuality?

And your logic ONLY has the Input of %I(AIA.CurrentQuality) configured? It doesn't care about any other inputs at all?


Reply User: Dmitriy, posted: 2019-03-04 12:14:11
other inputs ( .CurrentValue and etc.), do not have this case.