New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted
Lt. Commander

[import] ClearSCADA Protocol Support IEC61850

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: Craig_Scott, originally posted: 2019-08-19 05:59:36 Id:486
Has anyone seen ClearSCADA operating in an MV based application (protection relays / MV switchgear) using IEC61850 protocol? Any 3rd party drivers you know of that is suitable?


Reply User: geoffpatton, posted: 2019-08-19 13:59:23
I usually turn to kepware when ClearSCADA does not have a driver.They have a 61850 driver, i have not used it though.
I setup a substation that has 61580 the relays were using it to pass information to each other, but we used DNP3 for the SCADA. 61850 is only supposed to be used inside the substation.


Reply User: Craig_Scott, posted: 2019-08-19 23:26:52
Thanks for the advice Geoff


Reply User: geoffpatton, posted: 2019-08-20 16:56:48
You are welcome hope all goes well.