41288members
184238posts

Welcome to Geo SCADA Expert

Highlighted
Sisko

Welcome to Geo SCADA Expert

Dear All,

 

welcome to the Geo SCADA Expert Forum. We'll be growing the amount of information here, and also don't forget to consult the Resource Center for more information too.

 

The address of this has moved - it's now at: 

https://tprojects.schneider-electric.com/telemetry/

 

Thank-you!

5 REPLIES 5
Highlighted
Crewman

Re: Welcome to Geo SCADA Expert

That link does not appear to work.

Highlighted

Re: Welcome to Geo SCADA Expert

Excited to see another community on Exchange! 

Highlighted
Crewman

Re: Welcome to Geo SCADA Expert

The Resource Centre is currently down. They're working on it and hopefully it's back up and running soon.

 

In the meantime, here are download links to the last set of Monthly builds for June 2019.

 

ClearSCADA 2017 R3 June 2019 Update (80.7126.1)

Release Notes: https://schneider-electric.box.com/shared/static/8telpdlpzggn5hi2julncfr7hoa67v8m.pdf

Software Image: https://schneider-electric.box.com/shared/static/x68ud1w5upp8ypafractioaavxlb4izz.iso

 

ClearSCADA 2017 R2 June 2019 Update (79.7126.1)

Release Notes: https://schneider-electric.box.com/shared/static/haeqb15gakqmq2gmcxuz1h4oj04eooq7.pdf

Software Image: https://schneider-electric.box.com/shared/static/khzus14a6vu935w61i4u82dvi5fxlhhw.iso

 

ClearSCADA 2017 June 2019 Update (78.7119.1)

Release Notes: https://schneider-electric.box.com/shared/static/5fpcjr0cj767z3baj93ueypnn2bko33r.pdf

Software Image: https://schneider-electric.box.com/shared/static/shdf4bagr4qbh2cmf6caf43v1uq00u2f.iso

 

Updates are a combination of our Service Pack and Hotfix releases, rolled up into a single Monthly Update for each version, inclusive of recent bug fixes and put through the latest Windows Patch testing.

 

Each Update is a full installation just like the Initial Release – not a patch – which can be used to upgrade to the latest Monthly Update from a previous version (don’t forget to read the upgrade notes), or use to start a brand-new installation.

 

File Hashes

To be used as a separate source of verification which you can use to check that the downloads for ClearSCADA are correct. The SHA256 algorithm is used for ClearSCADA 2017 R2 on, with SHA1 used for previous releases. Use the command line ‘certUtil -hashfile pathToFileToCheck SHA256’ (or SHA1).

 

Release

Algorithm

Hash

ClearSCADA 2017 R3 June’19

SHA256

9DD99254AC1287661448897866701C2EB038EECB79D7BB88DFE997C0D1BDF528

ClearSCADA 2017 R2 June’19

SHA256

3994701C09009FB754A06DF0B89321955C3CFF0F70C23F4C9F135679CD0CCE98

ClearSCADA 2017 June’19

SHA1

8ab2fe35c4d88c51a1722739454a36c1e3bf4f87

Sisko

Re: Welcome to Geo SCADA Expert

Site move now complete - find it at: https://tprojects.schneider-electric.com/telemetry/

Highlighted

Re: Welcome to Geo SCADA Expert

Thanks for Sharing!!

EcoStruxure Geo SCADA Expert software is an integrated, scalable and reliable Supervisory Control and Data Acquisition (SCADA) software with ready-to-use telemetry features optimized for managing remote assets spread across the geographically dispersed infrastructure.

 

Read More: ERP Prep