New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
Make the most of your remote operations with end-to-end solutions with Process Automation’s SCADA and Telemetry Solutions. With the challenges that remote sites present, reliable communications for remote operation, monitoring & management are vital in enhancing productivity and ensuring profitability.
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Highlighted
Crewman

Using ServerObject.Interface to read array-based properties

Hi all,

 

Is it at all possible to read array-based properties using ServerObject.Interface in Scripting?

 

I am trying to read out the VectorValues property of a CProfileFloat profile object and populate a Form with the individual array values.

 

I can't get ServerObject.Interface to work at all as it complains about type mismatches.

 

I was doing something like:

 

Set FlowProfile = Server.FindObject(sFlowProfilePointFullName)

Vector1 = FlowProfile.Interface.VectorValues(0)

 

which did not work.

 

What is the correct way to do this?

3 REPLIES 3
Lieutenant JG

Re: Using ServerObject.Interface to read array-based properties

@rlao works for me...

 

Dim scxServer As ScxV6Server
Set scxServer = New ScxV6Server
scxServer.Connect "Test", "superuser", "superusersuperuser"
Dim objDoubleArray As ScxV6Object
Set objDoubleArray = scxServer.FindObject("New Float")

Dim arrDoubleArray
arrDoubleArray = objDoubleArray.Property("VectorValues")

 

[apologies for bad variable names etc etc... definitely awkward having an array called 'arrDoubleArray' that is full of 'Singles' ;)]

Ensign

Re: Using ServerObject.Interface to read array-based properties

The following JScript example works in a mimic script:

 

var Profile = Server.FindObject( "Time Profiles.Float" );
var Values = Profile.Interface.VectorValues;
var Times = Profile.Interface.VectorTimes;

var FirstValue = Values.getItem(0);
var FirstTime = Times.getItem(0);

 

I've not tried this from VBScript.

 


Andrew Scott, Lead Engineer, AVEVA
Crewman

Re: Using ServerObject.Interface to read array-based properties

Hi Andrew,

 

I'm trying to do this in VBScript, but your reply actually helped me figure out what I was doing wrong.

 

Basically, in addition to what I was doing in my original post, I was also trying to read VectorValues out into a ReDim variable sized to the MaxVectors of the float profile. Turns out that doesn't work and the solution was actually much, much simpler than what I was trying to do.

 

It was more or less like your JScript answer:

 

Set FlowProfile = Server.FindObject(sFlowProfileFullName)
Dim FlowArray
FlowArray = FlowArray.Interface.VectorValues

Flow1 = FlowArray(0)
Flow2 = FlowArray(1)
Flow3 = FlowArray(2) etc...

 

Extremely simple and I can't believe it took me this long to figure out.