In some previous (legacy) platforms we had the ability to embedded video (RTSP, HTML) typically though the old OLE/ActiveX platform.
We have used the Remote Image option to update snapshots on a specific interval or action, but a live video option would certainly be a great addition for some applications. With the new HTML5 Virtual Client now part of 2019, maybe progress will be made to implement a HTML5 Video element that can use the codecs available on the machine.
Just a simple request or suggestion, for now we launch a dedicated VMS viewer.
Solved! Go to Solution.
Since it appears Chromium/WebKit (Chrome, Edge (New), Operara, etc.) will now rule the world why not join the party with the integrated viewer:
Chromium Embedded Framework.
https://bitbucket.org/chromiumembedded/
Has links to using with .Net, Delphi, Java and others.
Allows embedding the web browser similar to how the ViewX currently embeds the IE ActiveX control.
A little bit of work and can keep security going.
Nearly every VMS and other machine vision camera works well inside a browser.
Allow a Inset window with the ViewX instead of only allowing a new or navigate and this will be easy to begin integration.
You can open hyperlinks to web pages in ViewX, so if the video is on a page already it should work.
Correct, you can force the default browser to open. We do this often to load external reporting and video connections
I am hoping more along the lines of embedding actual video in the mimic.
@JChamberlain thanks for sharing your thoughts .its working
Having an embedded video player within ViewX would still be good though 😉
Since it appears Chromium/WebKit (Chrome, Edge (New), Operara, etc.) will now rule the world why not join the party with the integrated viewer:
Chromium Embedded Framework.
https://bitbucket.org/chromiumembedded/
Has links to using with .Net, Delphi, Java and others.
Allows embedding the web browser similar to how the ViewX currently embeds the IE ActiveX control.
A little bit of work and can keep security going.
Nearly every VMS and other machine vision camera works well inside a browser.
Allow a Inset window with the ViewX instead of only allowing a new or navigate and this will be easy to begin integration.
I'm not sure that ViewX has ActiveX anymore. I know that it did have it (albeit unsupported) back in 2013 era (and prior), but I'm pretty sure when they migrated up to the 2014/2015 platform and had the major UI revamp it was dropped completely.
ViewX does actually already have a Chromium component, it's used to popout the GeoSpatial maps. But these also aren't capable of being embedded into a ViewX Mimic at this stage (although I've got a few feature requests that I've submitted around this).
Definitely worth sending in feature request tickets in my opinion (to your local Tech Support contact). Without feedback from End Users / System Integrators on what direction the product 'should' take, it becomes a guessing game for Schneider/AVEVA.
Interesting they would have Chromium support for the Geo/Maps but use the old OLE/ActiveX web component for displaying hyperlinks in ViewX:
I am aware they no longer allow ActiveX integration within the ViewX and dont want that back haha.
User | Count |
---|---|
188 | |
51 | |
16 | |
16 | |
14 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!