Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
RemoteConnect R2.5.1 for SCADAPack x70 now available on SHOP
EcoStruxure Geo SCADA Expert Forum
Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-01-2604:41 AM. Last Modified: 2023-05-0312:06 AM
RemoteConnect R2.5.1 for SCADAPack x70 now available on SHOP
Hello SCADA & Telemetry Community,
We are pleased to announce that RemoteConnect™ R2.5.1 for SCADAPack™ x70 is now available for download from SHOP.
RemoteConnect provides a flexible, easy-to-use programming and configuration environment for the SCADAPack x70 RTU series, which is comprised of the SCADAPack 470, 474, 570, 574 and 575 Smart RTUs. SCADAPack RTUs are closely integrated to work with Geo SCADA Expert.
New features in this update include:
SCADAPack 57x and 47x support for IEC 60870-5-104 protocol.
EFB Toolkit v14 supported by the logic editor. This feature allows adding custom C function blocks to the logic library, for use by SCADAPack x70 applications.
SCADAPack 47x and 57x support for 5505 RTD analog-input modules.
SCADAPack 47x and 57x support for 5410 counter-input modules.
SCADAPack 47x support for 6602 HART module with a limited feature set.
NETINFO command to provide additional diagnostics of IP connections.
Geo SCADA Import option for the SCADAPack 47x platform.
XEF and ZEF file formats added to the "Import Logic Project" option.
Support for SCADAPack 57x version 4 hardware in Boot loader and firmware.
GETDNPROUTE command to show DNP3 routes.
Software watchdog for logic tasks to improve behavior if a logic program contains an infinite loop or executes for an unexpected long time.
Support for side-by-side operation with Control Expert 15.
DNP3 device profile documentation updated.
Porting Guide for 'SCADAPack E-to-SCADAPack RemoteConnect' added to the documentation.