43332members
217764posts

Offline Map Geo SCADA / ClearSCADA

Highlighted
Commander

Offline Map Geo SCADA / ClearSCADA

Hi Everyone,

 

is it possible to make offline maps in ClearSCADA / GeoSCADA?

 

Thanks

Tags (2)
3 REPLIES 3
Highlighted
Commander

Re: Offline Map Geo SCADA / ClearSCADA

Hi @Oncom ,

I believe this has been discussed before on the old forums (the one in the middle anyway).

 

Within ClearSCADA this is not currently possible.

However it is possible to use an on-site caching WMS server.  There are a number of open source alternatives out there if you google it.  It would require some more work to set these up, and to appropriate configure caching, etc, but if security is a concern then this should be relatively easy to justify.

 

As WMS etc are layers over regular HTTP(S), then using a simple HTTPS application proxy (Web Proxy) should also be possible as a protection layer.  This would be much more simple to configure, but would require network traffic to be possible between the OT and 'Geo network'.

 

Regards,

Bevan


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
Highlighted
Lieutenant JG

Re: Offline Map Geo SCADA / ClearSCADA

I think you are referring to a post I started.

 

LINK EDITED BY STEVE:

https://community.exchange.se.com/t5/Geo-SCADA-Expert-Forum/Imported-GIS-Exportable-file-formats-sup...

Highlighted
Commander

Re: Offline Map Geo SCADA / ClearSCADA