>>Message imported from previous forum - Category:ClearSCADA Software<<
User: tcookson, originally posted: 2018-11-13 17:35:20 Id:317
I'm having an issue similar to, but not exactly like, the one described here: https://www.schneider-electric.us/en/faqs/FA275742/
If I follow the the FAQ note and add port 81, then mimics no longer display. In my case alarms/events/mimics all display correctly, but when I Hand Control a test internal point through WebX I get an error pop-up "not well-formed (invalid token)". WebX has control privileges in the web test folder, including the mimic I'm writing from and the point I'm trying to hand control.
System is ClearSCADA 2017 (Sept '17 update), running on Windows Server 2012.
Solved! Go to Solution.
>>Responses imported from previous forum
Reply From User: BevanWeiss, posted: 2019-01-03 21:59:34
Why would you change this from port 80 to port 81?
What port numbers (HTTP/HTTPS) is your WebX using?
NOTE: The FAQ is for "A common cause of these errors is the Original WebX being configured to use custom secure or non-secure ports". If you are not using 'custom secure or non-secure ports' then you should not have followed the directions in your link.
Reply From User: geoffpatton, posted: 2019-01-04 14:56:00
check the server configuration's WebX section and make sure Allow writes over HTTP is checked.
Reply From User: tcookson, posted: 2019-04-02 23:37:33
The check box states "Allow logon and database writes over ****non-secure ****HTTP.
I'd much prefer HTTPS, if possible.
Reply From User: sbeadle, posted: 2019-04-03 08:05:28
Client to web server communications are either HTTP or HTTPS, as configured within IIS. Web Server to ClearSCADA server communications are also configurable using HTTP or HTTPS, as configured in the IIS settings (referred in the FAQ) and Server Config tool WebX settings combined.
You can check the ClearSCADA server web port comms by enabling the WebX logging types in Server Status and reading the dbserver log files.
Reply From User: adamwoodland, posted: 2019-04-04 01:27:38
https://tprojects.schneider-electric.com/telemetry/display/CS/Diagnosing+Scripting+Connection+Errors may also help with your problem
>>Responses imported from previous forum
Reply From User: BevanWeiss, posted: 2019-01-03 21:59:34
Why would you change this from port 80 to port 81?
What port numbers (HTTP/HTTPS) is your WebX using?
NOTE: The FAQ is for "A common cause of these errors is the Original WebX being configured to use custom secure or non-secure ports". If you are not using 'custom secure or non-secure ports' then you should not have followed the directions in your link.
Reply From User: geoffpatton, posted: 2019-01-04 14:56:00
check the server configuration's WebX section and make sure Allow writes over HTTP is checked.
Reply From User: tcookson, posted: 2019-04-02 23:37:33
The check box states "Allow logon and database writes over ****non-secure ****HTTP.
I'd much prefer HTTPS, if possible.
Reply From User: sbeadle, posted: 2019-04-03 08:05:28
Client to web server communications are either HTTP or HTTPS, as configured within IIS. Web Server to ClearSCADA server communications are also configurable using HTTP or HTTPS, as configured in the IIS settings (referred in the FAQ) and Server Config tool WebX settings combined.
You can check the ClearSCADA server web port comms by enabling the WebX logging types in Server Status and reading the dbserver log files.
Reply From User: adamwoodland, posted: 2019-04-04 01:27:38
https://tprojects.schneider-electric.com/telemetry/display/CS/Diagnosing+Scripting+Connection+Errors may also help with your problem
User | Count |
---|---|
188 | |
52 | |
16 | |
16 | |
15 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!