>>Message imported from previous forum - Category:ClearSCADA Software<<
User: florian, originally posted: 2018-10-24 22:02:54 Id:210
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
----------------
**_ebennett:_**
**_Hi_**
**_I have setup the RTU to trend pulse counts every 15mins. One record logs the change and the other logs the current value.The RTU creates files which I can retrieve using E Configurator. In CS I have setup the Trend points and they only seem to update when I manually retrieve them by right clicking on the RTU, where do I set up the file uplad Frequency ?_**
**_Cheers_**
-------------
dmercer:
I've never used these before, but the help doc goves you this information at:
Driver Reference DNP3 SCADAPack E Driver Configuring DNP3 SCADAPack E Trend Sampler Functionality Example Configuration
The outstation should have SCADAPack Tab. In that tab under Trend Retrieval you can set when CS will retieve the tend data from the RTU.
---------------------
bevanweiss:
I would not recommend using Trend Points. They are incredibly specific to SCADAPack RTUs, and aren't really 'standard' in any means.
If you want a trend, you can get the same by using normal DNP3 points which are historised.
If you have the pulse counter feeding a DNP3 Counter point (as happens by default) then you just configure a Class against the counter, and a deadband for the events to be generated. When ClearSCADA does a poll then it will retrieve the DNP3 event records for the Counter point, and you'll have your trend available...
User | Count |
---|---|
188 | |
53 | |
16 | |
16 | |
15 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!