Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-11-0512:48 PM. Last Modified: 2023-05-0312:36 AM
[Imported] SVG of CS2017R1 Schema
>>Message imported from previous forum - Category:ClearSCADA Software<< User: florian, originally posted: 2018-10-24 20:58:13 Id:203 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
------------------
**_AWoodland:_** **_I found a generator over the weekend so I reused some old ClearSCADA code and generated the attached. Basically the schema hierarchy under CDBObject. SVG can be opened in a browser, no need for special software. All drivers installed except WITS._**
**_Hopefully it'll be useful should anyone need to explain the schema to anyone._**
------------------
bevanweiss: Thanks Adam Very cool. How was it generated? Did you just write some C# (or language of preference) to do recursion through the .NET API Classes? From memory it was difficult (impossible) to do this with the old Automation Interface..
-----------
**_AWoodland:_** **_Nothing very fancy, just parsed the XML tags from http://localhost/schema/cdbobject and a little bit of recursive programming, I'll clean the code up and post it. The original plan for the code was to generate a full structure including fields and methods that could be searched and driven down through... one day that might still happen but for now there is this SVG._**
**_There are other generators out there that take a - rather than a space, should be obvious in the code where to change that or do a global find and replace on a space in the output._**
**_No warranty with this code, use at own risk, etc._**
--------------------
**_AWoodland:_** **_Had more of a play, the attached might be useful for someone. Use Chrome or some HTML5 compliant browser (so pretty much anything but IE) as it uses HTML5 tags._**
**_Different from the SVG, creates a textual drill down from CDBObject for config, data and methods._**
**_Pretty horrid user experience with this to be honest, especially the colour picks, part of the whole generating these files is to play with the UI aspect._**