>>Message imported from previous forum - Category:ClearSCADA Software<<
User: ROVSCADAENGINEER, originally posted: 2019-05-30 23:33:42 Id:440
Would it be possible to add a new field as a string containing all the Tag names concatenated for FBD's
this would mean I can check that functionality within the DN consumes all specific points for regions. I can quickly locate any sites that such functionality is missing. Instead of visually inspecting each site.
If there is a query In which I can see this information any guidance would be greatly appreciated.
Solved! Go to Solution.
>>Responses imported from previous forum
Reply From User: sbeadle, posted: 2019-05-31 07:42:47
You can right-click a Logic program and display references. This will list references from and by the Logic, including those within the program. The Client .Net API also lets you call the same function from a program, so it's possible to write a simple program which lists references to a file.
Reply From User: ROVSCADAENGINEER, posted: 2019-06-02 21:27:38
yes that functionality is ok if you want to check individual sites. But for checking several sites at once I was meaning.
Reply From User: sbeadle, posted: 2019-06-03 10:58:47
I have placed an example utility to do this in a GitHub repository.
This example could be modified for any similar purpose.
https://github.com/ClearSCADA/utility-examples
Reply From User: ROVSCADAENGINEER, posted: 2019-06-05 00:59:12
Thanks for taking the time to do this beadle! very helpful.
Reply From User: sbeadle, posted: 2019-06-05 07:32:20
No problem.
Steve! .
>>Responses imported from previous forum
Reply From User: sbeadle, posted: 2019-05-31 07:42:47
You can right-click a Logic program and display references. This will list references from and by the Logic, including those within the program. The Client .Net API also lets you call the same function from a program, so it's possible to write a simple program which lists references to a file.
Reply From User: ROVSCADAENGINEER, posted: 2019-06-02 21:27:38
yes that functionality is ok if you want to check individual sites. But for checking several sites at once I was meaning.
Reply From User: sbeadle, posted: 2019-06-03 10:58:47
I have placed an example utility to do this in a GitHub repository.
This example could be modified for any similar purpose.
https://github.com/ClearSCADA/utility-examples
Reply From User: ROVSCADAENGINEER, posted: 2019-06-05 00:59:12
Thanks for taking the time to do this beadle! very helpful.
Reply From User: sbeadle, posted: 2019-06-05 07:32:20
No problem.
Steve! .
User | Count |
---|---|
188 | |
53 | |
16 | |
16 | |
15 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!