42311members
204641posts

[Imported] OPC DA Client showing BadOutoservice when connected to Clearscada

Sisko

[Imported] OPC DA Client showing BadOutoservice when connected to Clearscada

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: Shelin, originally posted: 2019-04-12 19:38:12 Id:404
Hi , Was trying to connect a third party OPC DA client to CLearscada using private security. Connection works fine I can see the tags that are permitted for the user. But when trying to read the current value the tag status says BadOutofService. Is this an permission issue on clearscada. i have given read control and review access for the user.