>>Message imported from previous forum - Category:ClearSCADA Software<<
User: Dmitriy, originally posted: 2018-11-29 14:44:08 Id:328
I have Logic ST in CS2017R2.
Execution Method - On Interval.
"Input Change detection" option selected in properties.
when i add input tag AT%I(IAI.CurrentQuality) IAI it is internal analog point, logic execute every time.
Solved! Go to Solution.
>>Responses imported from previous forum
Reply From User: Dmitriy, posted: 2018-12-03 08:22:26
i test them in CS 2013r2.3 - Logic execute one time.
Reply From User: BevanWeiss, posted: 2019-01-03 22:09:32
So you want it to execute at some interval, but to only run if the CurrentQuality is different from the previous CurrentQuality?
And your logic ONLY has the Input of %I(AIA.CurrentQuality) configured? It doesn't care about any other inputs at all?
Reply From User: Dmitriy, posted: 2019-03-04 12:14:11
other inputs ( .CurrentValue and etc.), do not have this case.
>>Responses imported from previous forum
Reply From User: Dmitriy, posted: 2018-12-03 08:22:26
i test them in CS 2013r2.3 - Logic execute one time.
Reply From User: BevanWeiss, posted: 2019-01-03 22:09:32
So you want it to execute at some interval, but to only run if the CurrentQuality is different from the previous CurrentQuality?
And your logic ONLY has the Input of %I(AIA.CurrentQuality) configured? It doesn't care about any other inputs at all?
Reply From User: Dmitriy, posted: 2019-03-04 12:14:11
other inputs ( .CurrentValue and etc.), do not have this case.
User | Count |
---|---|
188 | |
52 | |
16 | |
16 | |
15 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!