43429members
217967posts

[Imported] Hightlight database tree from Script

Highlighted
Sisko

[Imported] Hightlight database tree from Script

>>Message imported from previous forum - Category:Scripts and Tips<<
User: mchartrand, originally posted: 2018-10-23 17:22:17 Id:178
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

_________________

**_cmrl:
Hello,
(Thanks to geoffpatton for the suggestion to publish in this thread)
I need to find an object in the database, which is not a problem using: set obj = Server.LookUpObject(Id)
The challenge is how to highlight obj in the database tree in the current instance of ViewX from one script program?
It seems to be that the script world (Automation server, Mimic Scripts, COM, .NET) is separated from the current instance of ViewX ( the one that appears when the program is started).
There is an undocumented interface to ViewX, but this works only on created instances of ViewX.
Thank you for your help, Mauricio_**

___________________________

bevanweiss:
What you've asked for isn't really supported within ViewX.
You may be able to get this to work using the undocumented ViewX COM interface, but it wouldn't be recommended.

There is a context menu option 'Locate in Database Explorer', is this not essentially what you're trying to do?

-------------------------