Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2019-11-0501:58 PM. Last Modified: 2023-05-0312:33 AM
[Imported] Get the user Interface in Script
>>Message imported from previous forum - Category:Scripts and Tips<< User: mchartrand, originally posted: 2018-10-25 19:16:16 Id:276 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
_______
**_Dbaez: Hi, in a mimic script I am improving the visualization through: Set xvw = CreateObject("Serck.ViewXApplication") Of course I get an error in WebX when the PC doesn't have ViewX installed. How could I know if the user interface is ViewX or WebX? So in the WebX case I simply won't execute this part. Thanks for help :-)_**
_________________________
AWoodland: Use App.Head, if it returns 0 then its WebX, else returns the ViewX head id you're on (= 1).
The help has an example with Mimic.Close/back
________________
**_Dbaez: Thank you, it worked great. In the script, through the ViewXApplication I make some changes in the axes in the embedded trends. Now I'm wondering if it is possible to do this in WebX. So, The axes in embedded trends can be accessed using something different to ViewXApplication?_**