>>Message imported from previous forum - Category:ClearSCADA Software<<
User: KylePaynter123, originally posted: 2019-04-09 16:11:57 Id:402
Hi guys
Can anyone make sense of this error message ?
OBSOLETE-Use function in FPScripts to change faceplate.
I'm trying to tie a Faceplate to a mimic I did all the back end programming but when I click the mimic to get the faceplate the following is coming up as issue.
OBSOLETE-Use function in FPScripts to change faceplate.
Solved! Go to Solution.
>>Responses imported from previous forum
Reply From User: adamwoodland, posted: 2019-04-09 21:50:31
That looks like a custom generated MsgBox message, not something generated by the core software, check the script that is being called and see why its showing you that message.
Reply From User: KylePaynter123, posted: 2019-04-10 16:05:41
Thank you,
So basically you are saying to check the script to see if the script has any issues?
Reply From User: adamwoodland, posted: 2019-04-10 23:33:25
You should be able to just open the script and do a find on the text to find where it is.
The clue that it is not a standard ClearSCADA error message is that its not cryptic enough with random hex error codes 🙂
>>Responses imported from previous forum
Reply From User: adamwoodland, posted: 2019-04-09 21:50:31
That looks like a custom generated MsgBox message, not something generated by the core software, check the script that is being called and see why its showing you that message.
Reply From User: KylePaynter123, posted: 2019-04-10 16:05:41
Thank you,
So basically you are saying to check the script to see if the script has any issues?
Reply From User: adamwoodland, posted: 2019-04-10 23:33:25
You should be able to just open the script and do a find on the text to find where it is.
The clue that it is not a standard ClearSCADA error message is that its not cryptic enough with random hex error codes 🙂
User | Count |
---|---|
188 | |
52 | |
16 | |
16 | |
15 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!