>>Message imported from previous forum - Category:Bulk Edit Tool<<
User: <None>, originally posted: 2019-06-07 02:36:39 Id:444
The Bulk Edit tool doesn't seem to indicate the name of the Server that it is connected to. Does anyone know where to find this information?
Solved! Go to Solution.
>>Responses imported from previous forum
Reply From User: geoffpatton, posted: 2019-06-07 14:24:04
No there is nothing that shows this. It was originally developed to be run on the same computer as the server. When we tried using the first versions across the the network they timed out. That was back with 2009 versions of ClearSCADA. So we never had the need to see what server it was connected to, we knew.
Anyway it is now a Schneider product so you should contact your ClearSCADA technical support and put in a feature request. The simplest thing would be to have the Address displayed in the Title bar.
Reply From User: None, posted: 2019-06-12 19:02:45
Thanks Geoff. It will be a great to know what server it is connected to. I shall raise a feature request with Schneider Support
>>Responses imported from previous forum
Reply From User: geoffpatton, posted: 2019-06-07 14:24:04
No there is nothing that shows this. It was originally developed to be run on the same computer as the server. When we tried using the first versions across the the network they timed out. That was back with 2009 versions of ClearSCADA. So we never had the need to see what server it was connected to, we knew.
Anyway it is now a Schneider product so you should contact your ClearSCADA technical support and put in a feature request. The simplest thing would be to have the Address displayed in the Title bar.
Reply From User: None, posted: 2019-06-12 19:02:45
Thanks Geoff. It will be a great to know what server it is connected to. I shall raise a feature request with Schneider Support
User | Count |
---|---|
188 | |
53 | |
16 | |
16 | |
15 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!