New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Geo SCADA Expert Forum
Make the most of your remote operations with end-to-end solutions with Process Automation’s SCADA and Telemetry Solutions. With the challenges that remote sites present, reliable communications for remote operation, monitoring & management are vital in enhancing productivity and ensuring profitability.
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Sisko

[Imported] ClearSCADA Protocol Support IEC61850

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: Craig_Scott, originally posted: 2019-08-19 05:59:36 Id:486
Has anyone seen ClearSCADA operating in an MV based application (protection relays / MV switchgear) using IEC61850 protocol? Any 3rd party drivers you know of that is suitable?

1 REPLY 1
Highlighted
Sisko

Re: [Imported] ClearSCADA Protocol Support IEC61850

>>Responses imported from previous forum


Reply From User: geoffpatton, posted: 2019-08-19 13:59:23
I usually turn to kepware when ClearSCADA does not have a driver.They have a 61850 driver, i have not used it though.
I setup a substation that has 61580 the relays were using it to pass information to each other, but we used DNP3 for the SCADA. 61850 is only supposed to be used inside the substation.


Reply From User: Craig_Scott, posted: 2019-08-19 23:26:52
Thanks for the advice Geoff


Reply From User: geoffpatton, posted: 2019-08-20 16:56:48
You are welcome hope all goes well.