43494members
218076posts

[Imported] Bulk Edit Tool - Adding points / object to database

Highlighted
Sisko

[Imported] Bulk Edit Tool - Adding points / object to database

>>Message imported from previous forum - Category:Bulk Edit Tool<<
User: mchartrand, originally posted: 2018-10-19 13:25:40 Id:143
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum. The original posters' identities have not been included. Schneider Electric is not responsible for the content of these posts.

-------------------------------

**_Hi, I would like to know if it is possible to add new objects / points to existing ClearSCADA database using the bulk build tool.
Also please let know if seperate installable is available for download from any website?_**

-------------------------------

The BulkEdit only lets you edit existing objects.
The install is only available from the full ClearSCADA install. you can download the ClearSCADA install though. It is only available for the 2014 and greater versions.

This Excel add-in will probably do what you are looking to do. http://telemetry.schneider-ele...did=2603&enterthread=y