43546members
218143posts

[Imported] Automatic Guest log on

Highlighted
Sisko

[Imported] Automatic Guest log on

>>Message imported from previous forum - Category:ClearSCADA Software<<
User: KylePaynter123, originally posted: 2018-12-07 12:54:37 Id:334
Hi guys

Does anyone has any input as to how to program Clear Scada to open as a guest when opened

I saw some info on it but I think that deals more with which screens will be opened on a multi monitor system.

ps Clear scada works but users have to log on then log off for it to work as a guest.

1 REPLY 1
Highlighted
Sisko

Re: [Imported] Automatic Guest log on

>>Responses imported from previous forum


Reply From User: sbeadle, posted: 2018-12-07 13:53:01
Which ClearSCADA build and version (update month) are you using?


Reply From User: KylePaynter123, posted: 2018-12-07 15:14:33
hi,

Schneider Electric Clear SCADA 2017 R2

Clear SCADA User Interface

hope this info is useful


Reply From User: sbeadle, posted: 2018-12-07 15:19:44
See:
[Link](https://www.citect.schneider-electric.com/scada/clearscada/help/2017/Content/SecurityGuide/Definethe... "Link")

Remember to ensure that the Guest user has Read permission on the mimic and any children or data it carries.


Reply From User: KylePaynter123, posted: 2018-12-07 15:38:27
Thanks much will get to reading !


Reply From User: geoffpatton, posted: 2018-12-10 15:47:38
Did you go into File Options set the home page and then edit the Features of the guest user and select Display Home Page at logon. This has to be set on every Client computer and for each windows user that logs in and runs ViewX on each computer. In a domain setting I believe you can find the dat files ViewX uses and have those loaded when the user logs into windows.


Reply From User: sbeadle, posted: 2018-12-10 16:49:20
Does anyone have a few notes to add as to how to do this - reg settings, set up files etc?


Reply From User: adamwoodland, posted: 2018-12-11 03:20:39
The File Options is sadly still a binary .dat file, best way is to create one for your system, store it somewhere and copy as required, maybe a bat file which copies the file and starts ViewX rather than directly starting ViewX


Reply From User: KylePaynter123, posted: 2018-12-11 13:37:30
Ok guys,

The XML startup config needed some adjustments the XML

I tried the link that Sbeable suggested but that did not work

http://192.168.130.2/file/help_en-US/Default.htm#ClientAdministrationGuide/StartupConfigurationFile....


This URL link helped

Thank you guys