43453members
218021posts

Export-Import issue

Highlighted
Crewman

Export-Import issue

Hi,

 

It is me again...

I am currently experiencing difficulties with Geo SCADA.

I am in the development process of SCADA app and I have experienced many issues so far.

One of the issues is regarding exporting and importing objects.

I created a Group containing 7 ICMP digital points in order to have information if certain ethernet devices are available on the network.

Since I am having difficulties with copy-paste operations I decided to try everything on another machine. So I performed export of all items from main project folder. Then I imported all items to another Geo SCADA machine. I noticed that no ICMP digital points were imported. There is group tree created as it should be, ICMP group as well, but no ICMP digital points within ICMP group where they should be.

 

Am I doing something wrong?

 

 

 

 

2 REPLIES 2
Highlighted
Lieutenant

Re: Export-Import issue

What messages were displayed in ViewX when you imported the SDE file?

 

It sounds like the ICMP driver isn't installed on the second machine and so the ICMP objects is the SDE file couldn't be imported and so were discarded. If this is the case then there will be an error message for each object that couldn't be created.

 


Andrew Scott, Lead Engineer, AVEVA
Highlighted
Crewman

Re: Export-Import issue

@AndrewScott 

Thanks.