Hi,
It is me again...
I am currently experiencing difficulties with Geo SCADA.
I am in the development process of SCADA app and I have experienced many issues so far.
One of the issues is regarding exporting and importing objects.
I created a Group containing 7 ICMP digital points in order to have information if certain ethernet devices are available on the network.
Since I am having difficulties with copy-paste operations I decided to try everything on another machine. So I performed export of all items from main project folder. Then I imported all items to another Geo SCADA machine. I noticed that no ICMP digital points were imported. There is group tree created as it should be, ICMP group as well, but no ICMP digital points within ICMP group where they should be.
Am I doing something wrong?
Solved! Go to Solution.
What messages were displayed in ViewX when you imported the SDE file?
It sounds like the ICMP driver isn't installed on the second machine and so the ICMP objects is the SDE file couldn't be imported and so were discarded. If this is the case then there will be an error message for each object that couldn't be created.
What messages were displayed in ViewX when you imported the SDE file?
It sounds like the ICMP driver isn't installed on the second machine and so the ICMP objects is the SDE file couldn't be imported and so were discarded. If this is the case then there will be an error message for each object that couldn't be created.
User | Count |
---|---|
188 | |
51 | |
16 | |
16 | |
14 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!